Post Go back to editing

About ADP2389 Accuracy and minus current

Hi, 

I would like to use ADP2389.

So, I have two questions.

#1  When RILIM = 59 kΩ, the peak current is stated as 15 ~ 18.6 A. (From data sheet)
    Is this variation in output peak current equivalent (about ± 10.7%) even if the resistance value is changed?
       Are there any indicators?

#2   Is there any problem if a negative current flows in the FET of ADP 2389?

Best Regards,

Yuya

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.