Post Go back to editing

Formula for ADR0x TRIM resistors

Thread Summary

The user seeks to use fixed resistors instead of a potentiometer to set the ADR01 output to 10.03V. The final answer explains that while a formula for resistor values is not provided, using a potentiometer is recommended due to resistor tolerances and initial voltage errors. The user is using the ADR01 for a 10V reference input to a DAC, with an AMP03 for the -10V reference, and needs the 10.03V to compensate for filter-induced attenuation.
AI Generated Content

I would like to use the TRIM pin with fixed resistors rather than a potentiometer to set the ADR01 output to a voltage other than nominal, within the specified adjustment range.  Is there a formula to determine the appropriate resistor values?  I could breadboard it then measure the potentiometer setting, but if you can provide a formula, that would be quicker and easier.

Parents
  • I am using the ADR01 to generate a 10V reference input to a DAC.  I am using an AMP03 to produce the -10V reference.  I was getting some glitch noise on the DAC output, so, I added a lowpass filter to the negative reference input.  The reference input has an input resistance, so my filter was causing a slight attenuation in the reference voltage.  The 10.03V figure is to compensate for this loss.

Reply
  • I am using the ADR01 to generate a 10V reference input to a DAC.  I am using an AMP03 to produce the -10V reference.  I was getting some glitch noise on the DAC output, so, I added a lowpass filter to the negative reference input.  The reference input has an input resistance, so my filter was causing a slight attenuation in the reference voltage.  The 10.03V figure is to compensate for this loss.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.