Hi
Suggest a constant current regulator which can source 20A current and support a voltage output of minimum 100V.
If modification is made, can i use LT3763 to operate at 100V like by using GATE drivers.
Regards
Bivin George
LT3763
Production
The LT3763 is a fixed frequency, synchronous, step-down DC/DC controller designed to accurately regulate output currents up to 20A. The average current...
Datasheet
LT3763 on Analog.com
Hi
Suggest a constant current regulator which can source 20A current and support a voltage output of minimum 100V.
If modification is made, can i use LT3763 to operate at 100V like by using GATE drivers.
Regards
Bivin George
Hi, Bivin,
Basically, if the output current reaches the set output current limit, the output current loop will function and make sure it won't go beyond. Otherwise the voltage loop will function to regulate the output voltage. If you have a voltage source output such as a battery, by setting the regulated output voltage higher than the battery voltage, you can make the converter operating as a constant current source with the current equal to the output current limit. For more detailed spec. related questions, please contact our local FAE for more help.
Regards,
Jeoffrey
Hi, Bivin,
Basically, if the output current reaches the set output current limit, the output current loop will function and make sure it won't go beyond. Otherwise the voltage loop will function to regulate the output voltage. If you have a voltage source output such as a battery, by setting the regulated output voltage higher than the battery voltage, you can make the converter operating as a constant current source with the current equal to the output current limit. For more detailed spec. related questions, please contact our local FAE for more help.
Regards,
Jeoffrey