Hi
Suggest a constant current regulator which can source 20A current and support a voltage output of minimum 100V.
If modification is made, can i use LT3763 to operate at 100V like by using GATE drivers.
Regards
Bivin George
LT3763
Production
The LT3763 is a fixed frequency, synchronous, step-down DC/DC controller designed to accurately regulate output currents up to 20A. The average current...
Datasheet
LT3763 on Analog.com
Hi
Suggest a constant current regulator which can source 20A current and support a voltage output of minimum 100V.
If modification is made, can i use LT3763 to operate at 100V like by using GATE drivers.
Regards
Bivin George
Hi
In LTC3779 data-sheet it is mentioned, " Constant-Current Regulation (IAVGSNSP and IAVGSNSN Pins)The LTC3779 provides a constant-current regulation loop for either input or output current. A sensing resistor close to the input or output capacitor will sense the input or output current. When the current exceeds the programmed current limit, the voltage on the ITH pin will be pulled down to maintain the desired maximum input or output current. "
Kindly explain the above.
Also Fil mentioned that " The only IC to survive 100V output is LTC3779 which can also work as a current source. "
If LTC3779 can't be used, suggest an IC which can be used as constant current regulator to regulate current of 14A at 100V.
What about LT3796 or LT3756 IC to regulate current at 100V with 14A. Please reply asap.
Regards
Bivin George
Hi
In LTC3779 data-sheet it is mentioned, " Constant-Current Regulation (IAVGSNSP and IAVGSNSN Pins)The LTC3779 provides a constant-current regulation loop for either input or output current. A sensing resistor close to the input or output capacitor will sense the input or output current. When the current exceeds the programmed current limit, the voltage on the ITH pin will be pulled down to maintain the desired maximum input or output current. "
Kindly explain the above.
Also Fil mentioned that " The only IC to survive 100V output is LTC3779 which can also work as a current source. "
If LTC3779 can't be used, suggest an IC which can be used as constant current regulator to regulate current of 14A at 100V.
What about LT3796 or LT3756 IC to regulate current at 100V with 14A. Please reply asap.
Regards
Bivin George