Hi
Among regulators LT3796, LTC3779 & LT3756 which is the best regulator to implement a Constant current source with an output voltage of 96V. Suggest if any better regulators are available.
Regards & Thanks
Bivin George
LT3756
Production
The LT3756, LT3756-1 and LT3756-2 are DC/DC controllers designed to operate as a constant-current source for driving high current LEDs. They drive a low...
Datasheet
LT3756 on Analog.com
LT3796
Production
The LT3796/LT3796-1 are DC/DC controllers designed to regulate a constant-current or constant-voltage and are ideal for driving LEDs. The fixed frequency...
Datasheet
LT3796 on Analog.com
LTC3779
Recommended for New Designs
The LTC3779 is a high performance buck-boost switching regulator controller that operates from input voltages above, below or equal to the output voltage...
Datasheet
LTC3779 on Analog.com
Hi
Among regulators LT3796, LTC3779 & LT3756 which is the best regulator to implement a Constant current source with an output voltage of 96V. Suggest if any better regulators are available.
Regards & Thanks
Bivin George
Hi Fil
Input will be 100V with 12A supply. I need to generate a constant current source of 12A with 100V capability.
Note : voltage given as input can be more but input current remains minimum 12A.
Regards & Thanks
Bivin George
Hi Fil
Input will be 100V with 12A supply. I need to generate a constant current source of 12A with 100V capability.
Note : voltage given as input can be more but input current remains minimum 12A.
Regards & Thanks
Bivin George