Hi
Among regulators LT3796, LTC3779 & LT3756 which is the best regulator to implement a Constant current source with an output voltage of 96V. Suggest if any better regulators are available.
Regards & Thanks
Bivin George
LT3756
Production
The LT3756, LT3756-1 and LT3756-2 are DC/DC controllers designed to operate as a constant-current source for driving high current LEDs. They drive a low...
Datasheet
LT3756 on Analog.com
LT3796
Production
The LT3796/LT3796-1 are DC/DC controllers designed to regulate a constant-current or constant-voltage and are ideal for driving LEDs. The fixed frequency...
Datasheet
LT3796 on Analog.com
LTC3779
Recommended for New Designs
The LTC3779 is a high performance buck-boost switching regulator controller that operates from input voltages above, below or equal to the output voltage...
Datasheet
LTC3779 on Analog.com
Hi
Among regulators LT3796, LTC3779 & LT3756 which is the best regulator to implement a Constant current source with an output voltage of 96V. Suggest if any better regulators are available.
Regards & Thanks
Bivin George
Hi Bivin,
It would help if you can identify what application is your design for and what are the input supply specs.
Hi Fil
Input will be 100V with 12A supply. I need to generate a constant current source of 12A with 100V capability.
Note : voltage given as input can be more but input current remains minimum 12A.
Regards & Thanks
Bivin George
Hi Bivin,
I cannot find an existing solution that's why I recommend that you contact local support to help understand your requirement.
Thanks!