Post Go back to editing

450V with 1mA generation from an input voltage of 5V to 12V input

Hi

Suggest a regulator which can generate 450V output with 1mA output current from a source with minimum 5V to maximum 12V input.

Regards & Thanks

Bivin George

Parents Reply Children
  • Hello i have a problem with this 400V output design

    My problem is; i can not find the transformer (''13324-T087'' by Sumida Corporation,) in digikey, rs component, mouser or any other..

    I need to buy not 200 pieces, just 5 or 10 piece.

    Is there anyone can help me to cover that problem, i will change my whole design if i can not find this component.