Post Go back to editing

ADP2442 shutdown output after some seconds

Hi!

We are evaluating the ADP2442 ic. Our prototype is a basic dc dc converter, from 24V to 5V

This is the schematic (basically a copy&paste of the reference design):

If we connect the pin 6 (SYNC/MODE) to gnd (pulse skip mode), the circuit seems to work. We have 5V and we can supply current for a test load.

But if we use the fixed mode (pin 6 to vcc), the circuit works for a couple of seconds, and then, it shutdowns. We were looking for something strange, but at first, we dont see anything.

any idea or suggestion?

Thank you very much!!!

Parents
  • I noticed that the AGND and PGND are connected together through pin13, that should be fine. Then the layout has no strange things.

    Did you encounter this "shut down" issue on every unit, or just this particular one?

    For the skip mode, have you tried to draw some load current to see if the ADP2442 can enter into FPWM mode smoothly?

    For the external LED, since the PGOOD is open-drain and when output is ready, it becomes high-Z. According to the schematic, the LED connection is not correct. Whatever the PGOOD is pulled low or released (high-Z), the LED will not be ON.

Reply
  • I noticed that the AGND and PGND are connected together through pin13, that should be fine. Then the layout has no strange things.

    Did you encounter this "shut down" issue on every unit, or just this particular one?

    For the skip mode, have you tried to draw some load current to see if the ADP2442 can enter into FPWM mode smoothly?

    For the external LED, since the PGOOD is open-drain and when output is ready, it becomes high-Z. According to the schematic, the LED connection is not correct. Whatever the PGOOD is pulled low or released (high-Z), the LED will not be ON.

Children
No Data