Post Go back to editing

ADP2442 shutdown output after some seconds

Hi!

We are evaluating the ADP2442 ic. Our prototype is a basic dc dc converter, from 24V to 5V

This is the schematic (basically a copy&paste of the reference design):

If we connect the pin 6 (SYNC/MODE) to gnd (pulse skip mode), the circuit seems to work. We have 5V and we can supply current for a test load.

But if we use the fixed mode (pin 6 to vcc), the circuit works for a couple of seconds, and then, it shutdowns. We were looking for something strange, but at first, we dont see anything.

any idea or suggestion?

Thank you very much!!!

Parents
  • Thank you for your reply!!

    AGND and PNGD are connected under the ic. You can see it on the schematics, on the pin 13. I followed the layout guidelines for this. Do you see anything strange here then?

    We damaged the chip doing tests (short playing with the multimeter pin) and we are waiting for a new one. I will post more infor about this. But I remember using a led to drive some current, with the same result.

    For sure, with no load, the ADP2442  shutdown after 3 or 4 seconds in fixed mode.

    Also, in skip mode and fixed mode, the LED on the PGOOD pin does not turn on :/ that is the most disturbing issue here.

Reply
  • Thank you for your reply!!

    AGND and PNGD are connected under the ic. You can see it on the schematics, on the pin 13. I followed the layout guidelines for this. Do you see anything strange here then?

    We damaged the chip doing tests (short playing with the multimeter pin) and we are waiting for a new one. I will post more infor about this. But I remember using a led to drive some current, with the same result.

    For sure, with no load, the ADP2442  shutdown after 3 or 4 seconds in fixed mode.

    Also, in skip mode and fixed mode, the LED on the PGOOD pin does not turn on :/ that is the most disturbing issue here.

Children
No Data