Post Go back to editing

ADP2442 shutdown output after some seconds

Hi!

We are evaluating the ADP2442 ic. Our prototype is a basic dc dc converter, from 24V to 5V

This is the schematic (basically a copy&paste of the reference design):

If we connect the pin 6 (SYNC/MODE) to gnd (pulse skip mode), the circuit seems to work. We have 5V and we can supply current for a test load.

But if we use the fixed mode (pin 6 to vcc), the circuit works for a couple of seconds, and then, it shutdowns. We were looking for something strange, but at first, we dont see anything.

any idea or suggestion?

Thank you very much!!!

Parents
  • Hi,

    The schematic looks fine. For the layout, it seems that the AGND and PGND planes are not connected together on the PCB?

    When doing PCB layout, it is fine the separate AGND and PGND. But usually, we will connect these two ground planes on the PCB board.

    Another thing is, when setting to FPWM mode, how many load did you draw from Vout or even under no load condition, the ADP2442 will shut down after a while?

    Thanks!

Reply
  • Hi,

    The schematic looks fine. For the layout, it seems that the AGND and PGND planes are not connected together on the PCB?

    When doing PCB layout, it is fine the separate AGND and PGND. But usually, we will connect these two ground planes on the PCB board.

    Another thing is, when setting to FPWM mode, how many load did you draw from Vout or even under no load condition, the ADP2442 will shut down after a while?

    Thanks!

Children
No Data