Post Go back to editing

Will LTC1981 drive two in series MOSFETs?

I am design an smart LiPo power pack for an existing device. I need  to switch on/off a LiPo cell (3.7V) from its charger and power path controller used in the existing device.

For tjat I'm intending to use a LTC1981 in the following configuration.

A bidirectional switch is necessary because the PMIC in the existing device will charge the battery when +5V is present and connect the battery to the power rail when +5V is not present.

The current will be no more than 1 A and the LTC1981 will be controlled by a tiny micro-controller powered by the battery itself.

Do you think that LTC1981 will be able to control the two MOSFETs providing a bidirectional on/off switch?

Best regards

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.