KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
LTC1981
Production
The LTC1981/LTC1982 are low-power, self-contained N-channel MOSFET drivers. An internal voltage tripler allows gates to be driven without the use of any...
Datasheet
LTC1981 on Analog.com
I am design an smart LiPo power pack for an existing device. I need to switch on/off a LiPo cell (3.7V) from its charger and power path controller used in the existing device.
For tjat I'm intending to use a LTC1981 in the following configuration.
A bidirectional switch is necessary because the PMIC in the existing device will charge the battery when +5V is present and connect the battery to the power rail when +5V is not present.
The current will be no more than 1 A and the LTC1981 will be controlled by a tiny micro-controller powered by the battery itself.
Do you think that LTC1981 will be able to control the two MOSFETs providing a bidirectional on/off switch?
Best regards
afmenhem
What company do you represent and what's annual quantity of this project?
The LTC1981 was not designed to drive back-to-back MOSFETs, it is not in datasheet. Generally speaking, though, you can do this, below is LTspice simulation of the discussed circuit. The biggest problem is relatively long turn on/off. Also, we did not tested LTC1981 in this configuration.
You might look at LTC4412 with configuration on page 11, Figure 4. You can use related DC1635A to test your circuit on the bench.