ADP1755 output voltage drift

Hi all, 

I use ADP1755 to generate the 1.3 V for AD9364. 

Based on the ad_fmcomms3_reva schematic, I design the AD1755 circuit to convert 2.5V to 1.3V as the following.

PS: D1V5 means 2.5 V source voltage.  

For the larger board, everything works correctly. 

However, for the smaller board, the output voltage is 1.5V, not 1.3V without loading. 

I try to change R10 and R8 to 100K and 160K, but the output voltage is still 1.5V 

Please show me clue to solve this problem ? 

thanks 

ad-fmcomms3_reva.pdf
Parents Reply Children
No Data