LT8330 absolute maximum rating between EN/UVLO and VIN

Hello

What is reason which  EN/UVLO Pin Above VIN Pin is 6V?

If between EN/UVLO and VIN apply above 6V then damage may occur on LT8330?

Is this voltage protection diode breakdown voltage?

Best Regards

T. Kamino

Parents
  • The LT8330 designer told me previously that 6V was deliberately chosen as the abs. max. voltage for the "EN/UVLO Pin Above VIN Pin" rating.  I don't think the 6V rating is due to a protection diode breakdown voltage, but customers should avoid more than 6V from EN/OVLO to VIN on the LT8330. 

Reply
  • The LT8330 designer told me previously that 6V was deliberately chosen as the abs. max. voltage for the "EN/UVLO Pin Above VIN Pin" rating.  I don't think the 6V rating is due to a protection diode breakdown voltage, but customers should avoid more than 6V from EN/OVLO to VIN on the LT8330. 

Children
No Data