Post Go back to editing

LT8609EMSE#PBF Step down regulator

Hello, 

Is my first time with the LT8609 regulator and i'm really disappointed. I copied exactly the same design of the typical application described on the first page of it Datasheet, and it doesn´t really works as expected

My VCC is an wall adaptar of 12V @ 2.1A.  

The only circuit to which i'm supplying voltage is a Raspberry Pi Zero W. According with the current measurement there is about in average around 150mA and the voltage of the source down until 3.5V restarting the Raspberry. At this point, all is a mess and a scam, because as you can see on the following image the ouput supports supposedly  2A at 5V.

I selected this regulator because i have another projects with the LT3995EM and this have been working perfectly always, but i thought that 3A output would be too much for this project. 

So, what i have done:

  • First, i changed the 187K for one of 182K because with this first the voltage output is 4.96V, not 5V. 
  • I changed the RT resistor to a 182k and the Raspberry is working good without restarting; but, the output voltage down to 4.65V and is unstable. I'm measuring some ADC points and the values are oscillanting because of this behavior. 
  • Now, and trying to fix the unstable output voltage i change the RT to 47K and the voltage mantains stable in 5V but once i turn on the WIFI of the Raspberry, this do not work as expected, i suppose this is because that the source does not supply enough current. 
  • Trying to find the solutions to my problems i follow the design of my LT3993. This can be detailed on the following image. So i punt the SYNC pin to GND. The PG resistor i removed it, and the SS pin os to GND across a 10nF capacitor. But it didn't solve my troubles. 

Finally in order to discard the regulator, i did an adaptation and i connected with wires the LT3995 supply source (as detailed on the image above) to the main board where i have the Raspberry, and everything works fine! Current and voltage stabilization. But THIS IS NOT MY SOLUTION.

So i would like to you help me to solve this trouble with the LT8609, i dont know what else to do.

Thanks!!!

  • 1. Firstly please make sure the input VCC is a stable 12V when the issue happens.

    2. Please make sure all components on you board have correct value, for example C1 is 0.1uF, not 0.1nF.

    Below is the demo manual for standard demo board. In page 6 you can find the BOM.

    http://www.analog.com/media/en/dsp-documentation/evaluation-kit-manuals/dc2195afb.pdf

    3. Please compare your components voltage & current rating with the BOM, espically the input & output capacitors and inductor.

    4. Please double check your soldering has no problem.

    5. You may restore RT to 18.2k, otherwise you need to change inductor and output capacitor accordingly.

    If it still doesn't work after these 5 steps, you may need to replace a new IC.

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
  • hi,my design is the same as above.And i check the property of all the compents again and again. In order to verify the design can output 2A current,i connect the resistance (value 3Ω 100w)。when the input voltage is 5-8.5v,the output voltage is 4.76v ,electric current is 1.3-1.57A.  when the input voltage is 8.5 above,the output voltage is 2.86v-3v,the electric current is 0.78A!

    I test again and again,this problem existed all the time!What should i do!

    Thanks!