ADP5092 configuration

Hi EZ, 

I am currently trying to re-configure the ADP5092. This is the behavior that I am looking for :

-Vsys = 2.4V constant to power up my microprocessor

-Reg_out = 3.6V constant to power up another ADP

According to the datasheet, if I want to fix Reg_out = 3.6V I have to set Rvid to 27.7kOhm (currently 55.6kOhm on my schematic as I was delivering 3.3V before).

For fixing Vsys, according to the datasheet there is this formula : 

  • Vref is supposed to be fixed around 1V according to the datasheet, but when I look at the voltage on the oscilloscope I can only see this signal, do you have an explanation for this ?  

  • The thing that I don't get is that Vbat = Vsys, do you have an idea how to change this ? 

Here is the current schematic that I am using : 

Thanks for your help,

Florent