LTC4001 not working

Hello Sir,

We are designing a charger for our application where we have used LTC4001 IC. We are getting 1.213V at PROG and IDET pin but the output voltage is coming 3.012V only. 

Any suggestion or idea what to do?

  • 0
    •  Analog Employees 
    on May 2, 2018 5:37 PM

    Hello,

    Is this operation with or without a battery attached? This particular part was designed to operate with the battery attached.

    If the battery is attahced is there a fault indicated on the Fault pin or temperature fault indicated on the /CHRG pin?

    I also notice that the schematic only shows a 0.1uF on VIN. Is there a 10uF on the VIN pin not shown? (This is not related to the problem.)

    Thanks

  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:04 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin