Hello everyone,
I am currently using a LTC1760 that communicates via SMBus with a microcontroller. I developed my own pcb based on the reference design given in the datasheet.
The configuration:
I adapted the resistance bridges giving on the LOPWR pins, and DCDIV to my project.
Vmode = Vcc2 and Vdds> Vih_vdds (2.6V) -> Normal Operation on all, Charging is Allowed
The LTC1760 is connected either to the wall adapter or to a battery of (Smart Battery). The Power Switch works very well. If I feed the circuit with the wall adapter, the circuit is powered with the voltage supplied by the wall adapter and if I power with a smart battery the circuit is powered with the battery voltage.
My problem is on the side of the charge and the SMBus. The charger is not working and my SMBus levels are not consistent. let me explain :
The circuit detects well the battery or the wall adpateur but when both are present the charger is not working
SMBus Signal: SMBus ALERT = LOW SDA = 0.7V and SCL = 0.7V
Any ideas ???????
Thanks in advance !