Hello everybody,
I'm working on a boost converter, used to boost a 400V input voltage up to 550V.
The circuit is build around the LTC3805 but I figure out mainly a startup problem: after the controller issues 4-5 pulses, it stop to work. After some seconds, it tries to restart, stops again and the sequence repeats indefinitely. Reading the datasheet, seems to be a hiccup mode triggered by an overcurrent; but this should not be as the OC pin is directly connected to GND.
What else may trigger an overcurrent or stopping the controller?
Power supply voltage and RUN signal are OK, the circuit is realized on a 4-layers board with all the GND pads directly connected to a ground plane.
The simulation of the circuit does not exibith any problem.
Any suggestion will be appreciated; thank you in advance,
Marco.