Post Go back to editing

ADM1166 Input Voltage readback via I2C

adm1166

I wanted to read the input voltage on VP-AUX1 pins via I2C. I came across the below formula to calculate the voltage on the pins 

V = (ADCCode / 4096)
× Attenuation Factor × VREFIN

I was wondering what is the adc code here? Is the ADC values from the below registers ADC Value registers from Table 17.

VP1 0xA0    ADCHVP1    7:4 N/ANot used if 0x82[2] (average) = 0.
                                         0-3 OUT3 to OUT0
                                        R/W 4 MSBs of 12-bit result of ADC conversions on VP1 when 0x82[2] (average) = 0.
                                        7-0 OUT7 to OUT0

I am reading the values from this and trying to calculate but the calculated voltage appears to be wrong.

Please help.

Regards,

Djay

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.