Post Go back to editing

LTC1515 adjustable output voltage

Hello,

We have a design with an LTC1515 in it running the adjustable output version with VOUT at 7.4V (R1=100k; R2=20k) - the datasheet doesn't say much about VOUT for the adjustable part except for the absolute max at 12V. It has been looked at by an LT engineer but can someone confirm (as the other parts in the family are fixed 3V/3V3/5V) that the part should should be happy with an output set above 5V? We are seeing some parts (when VIN is around [8.2 - 8.6]V) fail (getting very hot an dieing) - the bench testing we've done definitely has not exceeded the 10V max VIN (won't have been above 9V).

Kind regards,
Dave