Limiting Inrush Current issue with LTC4367

I am using LTC4367 as inrush current limiter for my applicationwith IN of 36V. I am using a single power MOSFET as indicated in the attached LTSpice schematic to limit the inrush current into 4 HV electrolytic capacitors each of 560uF. There is no load connected at the output as the next converter stage is undervoltage protected with UV= 88% of VDC.
In order to limit the current to around 1.2A, I am using a 65nF capacitor at the gate shown. However, I cannot assure if the power MOSFET used (IPB048N15N5_L1) will still work in SOA because as shown in the waveform attached, both Id and Vds of the power MOSFET are ramping with time, thus I am not sure which time period at which voltage/current I should consider to check the SOA of the power MOSFET. The issue is that the using of Cgate of 65nF does limit the inrush current, however it prolongs the linear region operation of the power MOSFET.

Any comment please?
Thanks

P.S: The LTSpice schematic can be sent for testing.

Schematic Testbenchsimulation waveform