Post Go back to editing

LT8611 damaged with absent input voltage

Hello,

we are using the LT8611 for charging a 12V lead acid battery.

When the  24V input voltage is removed the LT8611 will be destroyed. 

We added a diode like the recommendation from the LT8611 datasheet (page 18, figure 5) but this didn´t prevent the fault of the LT8611 when the input voltage is absent.

The schematic is attached below.

Any help is greatly appreciated,

Thomas

PDF



correct spelling of Subject "damaged"
[edited by: ThomasStunder at 10:49 AM (GMT 0) on 3 Jul 2020]
Parents
  • Hi Thomas,

    Thanks for use of LT8611 and the information.

    One of the possible sources, which causes the damage in battery charging application, comes from the reserve current, suddenly stepping up the voltage stress and exceeding the allowed max voltages on some pins.

    The simple solution to this problem is to add a forward-biased diode between the output of the part and the battery.

    If additional information is needed, please let me know.

    Best regards,

    Chuan

Reply
  • Hi Thomas,

    Thanks for use of LT8611 and the information.

    One of the possible sources, which causes the damage in battery charging application, comes from the reserve current, suddenly stepping up the voltage stress and exceeding the allowed max voltages on some pins.

    The simple solution to this problem is to add a forward-biased diode between the output of the part and the battery.

    If additional information is needed, please let me know.

    Best regards,

    Chuan

Children
No Data