Post Go back to editing

Artwork of LT4270

hi team

My customer asked me the following.

600 mA load applied to the poe output, measured at 620 mA.

This is the reading of the register.
There is a difference from the actual load of the electric loader.
EVboard is measured in the same value as the electric loader.

If you raise the load value a little more, the board is shutdown.

Looking at PCB designs, the difference in current measurement of output in the order that is close to the device decreases slightly.

The circuit diagram is the same as the LTC4270 EVB.

https://www.analog.com/media/en/dsp-documentation/evaluation-kit-manuals/DC1840C.pdf
My customer has a strong suspicion of artwork.
Please review the circuit diagram and Artwork.

Also, could you tell me if there is a mandatory in the artwork?

PDF

3857.poe_pcb.zip

Thanks

Damon

Edit Notes

add mandatory in the artwork
[edited by: Damon Ahn at 7:59 AM (GMT 0) on 6 Jul 2020]
Parents
  • Hi Damon,

    Can you confirm the circumstances of the test you described? Is this a Class 4 power allocation that is drawing the 600mA / 620mA? This is right up to the maximum of the specification. The LTC4270/LTC4271 will cut off the current when it senses a voltage between 152mV and 168mV across the 0.25 Ohm sense resistor, this means a current as low as 608mA could cause the port to be disconnected.

    In regards to the artwork on the schematic, yes, it is important. The twelve sense resistors must be kelvin sensed and they all share the same low-side sense point. Please review the DC1840C Demo Manual and Layout files for an example layout for the sense resistors.

    https://www.analog.com/media/en/dsp-documentation/evaluation-kit-manuals/DC1840C.pdf

    Best Regards,

    Eric

Reply
  • Hi Damon,

    Can you confirm the circumstances of the test you described? Is this a Class 4 power allocation that is drawing the 600mA / 620mA? This is right up to the maximum of the specification. The LTC4270/LTC4271 will cut off the current when it senses a voltage between 152mV and 168mV across the 0.25 Ohm sense resistor, this means a current as low as 608mA could cause the port to be disconnected.

    In regards to the artwork on the schematic, yes, it is important. The twelve sense resistors must be kelvin sensed and they all share the same low-side sense point. Please review the DC1840C Demo Manual and Layout files for an example layout for the sense resistors.

    https://www.analog.com/media/en/dsp-documentation/evaluation-kit-manuals/DC1840C.pdf

    Best Regards,

    Eric

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.