LT3591
Production
The LT3591 is a fixed frequency step-up DC/DC converter speci?cally designed to drive up to ten white LEDs in series from a Li-Ion cell. Series connection...
Datasheet
LT3591 on Analog.com
Hello,
I've a question about the device LT3591.
Page 11 of the data sheet shows a design example with a separate power supply for VIN and the inductor (SW).
Both voltages are about 3.3V.
Can I use this design with input voltages of 3.3V for Vin and 15V for the inductor path?
And is there are problem to use a 10µF instead of an 4.7µF capacitor at the output!
Thanks