LT3741
Production
The LT3741 and LT3741-1 are fixed frequency synchronous step-down DC/DC controllers designed to accurately regulate the output current at up to 20A. The...
Datasheet
LT3741 on Analog.com
LT3763
Production
The LT3763 is a fixed frequency, synchronous, step-down DC/DC controller designed to accurately regulate output currents up to 20A. The average current...
Datasheet
LT3763 on Analog.com
LT3743
Production
The LT3743 is a fixed frequency synchronous step-down DC/DC controller designed to drive high current LEDs. The average current mode controller will maintain...
Datasheet
LT3743 on Analog.com
LT3795
Production
The LT3795 is a DC/DC controller designed to regulate a constant-current or constant-voltage and is ideal for driving LEDs. It drives a low side external...
Datasheet
LT3795 on Analog.com
Customers frequently ask me how to check the feedback loop stability of their LED drivers or other current regulators so I will answer in a REPLY post.
To check the feedback loop stability of an LED driver or other current regulator, use the CTRL input to command a step change in load current - usually from about half to about full output current. Then observe the output current and make sure the response to the CTRL step is critically damped. Adjust the feedback loop compensation if necessary. One image below shows this method appled to an example circuit schematic and there is also an image below of a scope capture that shows a stable LED current response.

Conditions for Scope Capture: LT3763EFE, mod DC1831A, 48VIN, 32VLED at 1.5A to 3A to 1.5A, ILED VCTRL transient_0.bmp

To check the feedback loop stability of an LED driver or other current regulator, use the CTRL input to command a step change in load current - usually from about half to about full output current. Then observe the output current and make sure the response to the CTRL step is critically damped. Adjust the feedback loop compensation if necessary. One image below shows this method appled to an example circuit schematic and there is also an image below of a scope capture that shows a stable LED current response.

Conditions for Scope Capture: LT3763EFE, mod DC1831A, 48VIN, 32VLED at 1.5A to 3A to 1.5A, ILED VCTRL transient_0.bmp