Hi,
I'm prototyping a PCB using the LT1962 and LT1611 voltage regulators, and I would like to run a simulation of the circuit in Autodesk EAGLE using a SPICE model. Do you have a SPICE model for these ICs?
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
LT1962
Recommended for New Designs
The LT1962 series are micropower, low noise, low dropout regulators. The devices are capable of supplying 300mA of output current with a dropout voltage...
Datasheet
LT1962 on Analog.com
LT1611
Production
The LT1611 is the industry’s first inverting 5-lead SOT-23 current mode DC/DC converter. Intended for use in small, low power applications, it operates...
Datasheet
LT1611 on Analog.com
Hi,
I'm prototyping a PCB using the LT1962 and LT1611 voltage regulators, and I would like to run a simulation of the circuit in Autodesk EAGLE using a SPICE model. Do you have a SPICE model for these ICs?