Post Go back to editing

Description of efficiency measurement in LTC3731 datasheet

Hi all,

 

I am asking about the Description of efficiency measurement in LTC3731 datasheet.

 

About temperature coefficient

 

In the formula for Pmain on page 27 of the data sheet, if the value of δ is calculated as [0.005*65] and the value of Rds(on) as 9 mΩ, the answer is 0.87W.

   

The value of Rds(on) at 90°C is multiplied by the temperature coefficient.

Is it correct?

 

②About values in expressions

 

Please tell me what should be substituted for (2) and (3) in the following equation.

   

Thanks

 

Takahiro

Parents Reply Children
No Data