KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADP7183
Recommended for New Designs
The ADP7183 is a complementary metal oxide semiconductor (CMOS), low dropout (LDO) linear regulator that operates from −2.0 V to −5.5 V and provides...
Datasheet
ADP7183 on Analog.com
Hi
I can't find the maximum operating voltage on the ADP7183's EN pin in the datasheet. I see that the absolute maximum voltage is +5.0 V but what is the operating maximum voltage?
Regards, Jonas
what is the operating maximum voltage?
Less than maximum rating.
As the threshold is much lower, there is no need to approach maximum rating.
Use a resistor devider for EN input if neccessary.
Hi Jonas,
You may operate the EN between +5V to -5.5V. Just make sure you won't exceed the absolute maximum ratings.
Best Regards,
Alex