Hello, I have a input protection requirement wherein the unit is subjected to negative 230V AC input.Though the LTC4251 datasheet won't specify usage for 230V maximum operating voltage,since it is a hotswap controller hope we can use this device -230 VAC input protection
As per our design requirement We have a negative AC rail wherein we are generating local negative supplies on board from negative AC rail(-48VAC). To suffice the protection against negative 230VAC requirement plan to this device
LTC4251-1IS6#PBF
Also I'm unable to buy this device at lower volumes from distributors.
Please clarify Whether LTC4251BIS6-1#TRMPBF can be used as replacement to LTC4251-1IS6#PBF
hope for spice model for LTC4251BIS6-1 is same as LTC4251-1
Thanks,
Phani.M