Can I current sink an LED on !PGOOD, LT3759?

Hello,

I can't find information in the datasheet on how much current the LT3759 !PGOOD pin can sink.  I am hoping to use this pin to light an LED (5mA) when it asserts LOW (indicating power is within 5%)

This is my schematic,

I also don't see a reason it has to be pulled high but all of the typical application examples show it pulled high..  So I did as well... Like I said earlier though, can I just put an LED on this !PGOOD pin (limited to about 5 mA).

Thank you!

-Chris

Parents Reply Children
No Data