Post Go back to editing

RUN/SS Pin Problem on LTC3878 and LTC 3729

Hi,

I want to use LTC3878 and LTC3729 in my design.These component have RUN/SS pin. Before advance design, I tried to simulate macro model in LTspice. Of course, these models operated properly. When Css (soft-start capacitor) was changed SS time increased and decreased  according capacitor value. But I am going to use enable signal for these component in design. I connected enable signal (logic signal) to RUN/SS pin , soft start time did not change for any capacitor value. When enable signal was applied output of component rapidly increased and overshoot occurred. How can I solve this problem? Is there any probability on spice model have a fault?

Best regards.

  • Hi ,

    as this input is for both SS and EN, you have to place the softstart cap here.
    If RUN/SS pin is below 1,5V the LTC3878 is disabled. To get additional EN/DIS you need a transistor (preferable small NMOS) from RUN/SS to GND that discharges the RUN/SS capacitor for disabling.

  • Thanks for your response. Your suggestion is second circuit,ı think. But I will use the PGOOD signal of another dc/dc converter. And this signal is active high. So when second circuit will be used my circuit will not work. When I simulated first circuit (except Vin and Rss) for RUN pin, Css started charging after active high signal. But ı do not have any information about selection D1 ( ı cant see any info in datasheet) diode and what is duty of D1 exactly?3729.asc

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.