Post Go back to editing

LT3008 part replacement

Hello,

I recently designed a board using the LT3008-5 to supply my 5V voltage rail, I am using the 8 lead TSOT-23 package.

It seems the electronics on the board consume more current than what the LT3008 series is rated for (20ma) and the device is not regulating properly. I was hoping that Analog Devices provides a 5V (an 4V - 8V will also work) LDO that supplies 150ma or more that is also an 8 lead TSOT-23 and has the same pinout as the fixed LT3008-5 regulator.

I don't mind that if its IQ is much larger than LT3008 series.

In the meantime I will be looking through the listed Analog Device LDOs on mouser.

Thank You 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.