LTC4215 I2C (minimum SCL frequency)

Hello!


The table in datasheet says that minimum SCL frequency is 400kHz (see table on page 5).
I care if that true because planned to use LTC4215 on the same bus with other device which can support I2C standard mode only (100kHZ maximum).

Regards,
Victor

Parents Reply
  • Hi Manpreet

    thanks for your feedback

    I also saw the note on the datasheet but that was a little confusing since there are 2 values for SCL(MAX) (is it is the MAX, why not just one?) and there is no mention of capability to work in I2C Standard or Fast Mode  along the datasheet.

    By chance, are you aware of any customer using this device at 100kHz?

    Thanks

Children
No Data