The voltage on the Vin (Pin34) and (CS, SG, DG and Vbias) pins can be different for normal oparation?
Can I limit the voltage on the pin Vin (Pin34) to 14V applying the series resistor and Zener diode like shown in figure 14 https://www.analog.com/media/en/technical-documentation/data-sheets/LTC3897-2.pdf and use 24V power supply which powers sircuits conected to pins CS, SG, DG, Vbias, RUN, SGEN, DGEN, IS+, IS-...?
On page 12 in this pdf is indicated when the ideal diode is used at the input to block negative input voltage, connect a Schottky diode from the VIN pin to the VBIAS pin, in this case, can I connect Vbias to IS- pin or another pins?