My Customer are reviewing the LT8606 ( buck Converter )
They use Brust Mode, Because Output Current is 10uA
They hope to improve the efficiency
- input : 10V ~ 15V
- Output :3.3V / 10uA
- Inductor : 6.8uH
in my opinion, at low load the switching frequency is lower than typical output current ( Brust Mode )
so, I think that if Inductor Value is higher than 6.8uH, efficiency is higher
anyway, I want to know another opinion!!
Pleaes Let me know~~ any opinion.... Thanks a lot