Post Go back to editing

LT3752 + LT8311 Stability

Hi,

I use the circuit of LT3752, that is on the ...LTspiceXVII\examples\jigs .

The circuit is not stable. It gets out of stabilization even when the output voltage is being build on the startup.

I tried to change capacitor+resistor that is connected to the COMP pin of LT8311, and the resistor that is connected to LT3752. But it stays unstabilized.

1-     Is there a way to make AC simulation (with LT3752 + LT8311) to check the Open loop parameters and close loop parameters?

2-     What is the right way to deside what is the right compensation network?

My design is:

  • Vin: 18-48
  • Vout: 15
  • Iout: 1.3A
  • Lout= 68uF
  • Cout= 4.7uF
  • Np=50uH Ns=200uH
  • f=500kHz

Best Regards,

Arkadi

Parents Reply
  • I want to use LT3752+LT3811 because of it's high efficiency. In addition, we are planning to make a few types of converters. Some of them more than 80W. 

    Anyway, the question is general. whether is LT3752+LT3811, LT3748 or something else.

    Is there a way to make AC simulation to check the Open loop parameters and close loop parameters?

Children