Post Go back to editing

Battery Temperature Qualified Charging of LTC4079 with extended temperature range from -35C to 80C.

Hi Zack,

Is it possible for LTC4079 to have more wider temperature range from -35C to 80C? For most NTC thermistors from Vishay or TDK, about 0C ~ 40C range following below threshold.

In my application, I'd like to extend temperature range to -35C to 80C.

Regards,

Ma Dawei

Parents
  • Hello,

    Yes, you can use a thermistor with a lower beta value for less sensitivity to temperature. This will effectively extend the NTC range based on the fixed threshold ratios that the LTC4079 uses. These ratios are given in the spec table to help assist you in choosing an alternate thermistor beta value:

    Regards,

    Zack

  • Zack,

    I calculated the Beta constant value needed following the threshold specified by spec of LTC4079, take 10K@25C NTC as an example. 1000K+ got. But TDK told me that they don't have NTC with 1000K+ products, all of their NTC products are with 3000K+ ~ 5000K.

    So that's my point, although theoretically it can be used in extended temperature range, but maybe no NTC products available now, I'm still waiting for Vishay feedback. Most likely, LTC4079 is designed to support most of battery chargers working in 0C ~ 40C temperature range.

    Regards,

    Ma Dawei

Reply
  • Zack,

    I calculated the Beta constant value needed following the threshold specified by spec of LTC4079, take 10K@25C NTC as an example. 1000K+ got. But TDK told me that they don't have NTC with 1000K+ products, all of their NTC products are with 3000K+ ~ 5000K.

    So that's my point, although theoretically it can be used in extended temperature range, but maybe no NTC products available now, I'm still waiting for Vishay feedback. Most likely, LTC4079 is designed to support most of battery chargers working in 0C ~ 40C temperature range.

    Regards,

    Ma Dawei

Children