Post Go back to editing

ltc4357 high current issue

Hi,
we work on a robotics system with two 48v Battery. I want to design a board in order to switch between two batteries with a load sharing system.

we need a circuit with a max 40A pike. I found LTC4357 for this work. but, can I use a high current Mosfet in this circuit for achieving more current?
Thanks

Parents
  • Hi,  Yes, you can use LTC4357 (or LTC4355 dual controller). You may need multiple parallel MOSFETs to limit power dissipation in each MOSFET. The load sharing will depend on copper trace and MOSFET resistances (aka droop sharing).

  • Thanks so much for your reply.

    how can I determine the threshold voltage between these two batteries for switching between them?

    I mean, want to have a circuit in which if a battery voltage equals 48V and the other equal 46 volts, the circuit continues the load sharing. that's important for me to share the current between two battery even if their voltage has a short difference.

    Thanks

Reply
  • Thanks so much for your reply.

    how can I determine the threshold voltage between these two batteries for switching between them?

    I mean, want to have a circuit in which if a battery voltage equals 48V and the other equal 46 volts, the circuit continues the load sharing. that's important for me to share the current between two battery even if their voltage has a short difference.

    Thanks

Children