hi,I use Input power 5V4A,want to get ±6V,1.5A,but I use ADP507x_DesignerTools,Remind me the maximum current is 1.25and.37,What am i doing wrong?
ADP5071
Recommended for New Designs
The ADP5071 is a dual high performance dc-to-dc regulator that generates independently regulated positive and negative rails.
The input voltage range of...
Datasheet
ADP5071 on Analog.com
hi,I use Input power 5V4A,want to get ±6V,1.5A,but I use ADP507x_DesignerTools,Remind me the maximum current is 1.25and.37,What am i doing wrong?
Hi roy,
2A and 1,2A are the switch rating not the output current rating and based on the inductor current peak. The excel file tool is good starting point for your design.
Hi roy,
2A and 1,2A are the switch rating not the output current rating and based on the inductor current peak. The excel file tool is good starting point for your design.
yes,excel file tool is very good,I understand it,thank you,If I want to achieve 5V4A to ± 6V,and has a large current output,have a good recommendation?
You may want to take a look at LT3757.