Post Go back to editing

A better part than MAX4420?

> I need some very low noise fully differential op-amps for amplifying a

> signal in the 10 M\Hz to 3 kHz range. Very low noise. For instance the

> MAX4420 is (surprisingly) not quite good enough. This takes the signal

> out of a ADL5387 demod and is the first amp stage and because dynamic

> range has to be maximized there is not a ton of amplification in the

> front end to overcome baseband amplifier noise.

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.