Post Go back to editing

A better part than MAX4420?

> I need some very low noise fully differential op-amps for amplifying a

> signal in the 10 M\Hz to 3 kHz range. Very low noise. For instance the

> MAX4420 is (surprisingly) not quite good enough. This takes the signal

> out of a ADL5387 demod and is the first amp stage and because dynamic

> range has to be maximized there is not a ton of amplification in the

> front end to overcome baseband amplifier noise.

Parents
  • FormerMember
    FormerMember
on Jun 12, 2015 7:23 PM
0

MAX4420 is a 6A MOSFET driver??

Harry


Reply
  • FormerMember
    FormerMember
on Jun 12, 2015 7:23 PM
0

MAX4420 is a 6A MOSFET driver??

Harry


Children
No Data