Dear Power by Linear,
I have a LT4256-2 output short test problem. The following circuit diagram is used for output short test. The test waveform shows that the short-circuit peak current exceeds 550A. But the SOA of the MOSFET I use is only 360A. How can I modify it to reduce the peak current of the output short to below 200A.
Thanks.