KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADP7112
Recommended for New Designs
The ADP7112 is a CMOS, low dropout (LDO) linear regulator that operates from 2.7 V to 20 V and provides up to 200 mA of output current. This high input...
Datasheet
ADP7112 on Analog.com
Hi,
from the datasheet of ADP7112 e.g. page 13, I understand that ANY ADP7112 version/model can be used in 'adjustable mode' providing the wanted output voltage is above the fixed voltage value.
However the ordering guide on page 21 listing the different versions only mentions the ADP7112ACBZ-1.2-R7 as 'adjustable' in the Output voltage column.
I would just like having the confirmation that ALL models, especially the ADP7112ACBZ-1.8-R7 which I plan to use, can be used in adjustable output configuration (w/ R divider).
Thank you
Francois Dorel