ADP7112
Recommended for New Designs
The ADP7112 is a CMOS, low dropout (LDO) linear regulator that operates from 2.7 V to 20 V and provides up to 200 mA of output current. This high input...
Datasheet
ADP7112 on Analog.com
Hi,
from the datasheet of ADP7112 e.g. page 13, I understand that ANY ADP7112 version/model can be used in 'adjustable mode' providing the wanted output voltage is above the fixed voltage value.
However the ordering guide on page 21 listing the different versions only mentions the ADP7112ACBZ-1.2-R7 as 'adjustable' in the Output voltage column.
I would just like having the confirmation that ALL models, especially the ADP7112ACBZ-1.8-R7 which I plan to use, can be used in adjustable output configuration (w/ R divider).
Thank you
Francois Dorel
Hi Francois,
To confirm, yes, all models of ADP7118, including the one you mentioned, can be used in adjustable mode via resistor divider by following the formula in Page 13.
Thank's a lot for the quick answer.
Thank's a lot for the quick answer.