The pictrue is schematic of LTM4609 evalutaion kits, Can I use a DAC such as AD5696 between R5 and R9 to program the output of LTM4609?
LTM4609
Recommended for New Designs
The LTM4609 is a high efficiency switching mode buckboost power supply. Included in the package are the switching controller, power FETs and support components...
Datasheet
LTM4609 on Analog.com
AD5696
Production
The AD5696, a member of the nanoDAC+™ family, is a low power, quad, 16-bit buffered voltage output DAC. The device includes a gain select pin giving...
Datasheet
AD5696 on Analog.com
The pictrue is schematic of LTM4609 evalutaion kits, Can I use a DAC such as AD5696 between R5 and R9 to program the output of LTM4609?
Yes this is possible. Note that typical FB injection scheme (ie below) de-grades load regulation if the adjustable output range is wide. If the output adjustable range is not wide then the below setup should be sufficient (Vg is DAC output).
If the adjustable output voltage is wide, to maintain good load regulation it would be recommended to insert an external error amp / compensator circuit to over-ride the internal error amp. Below is an example design verified for 0.5Vout - 15Vout adjustable output voltage. Thanks.
Thank you very much!
Hi, Young,
I'm just trying to do the same thing. Could you kindly post the high resolution picture or just upload the pdf version? Thanks!