Post Go back to editing

ltc4413-2

Hello

I am going to work with four power supplies and i want to make ORing with them' so that the greater of them will "win".

the inputs voltage are:

  1. 4.1-3.5V (battery)
  2. 4.1-3.5V (battery)
  3. 3.7V
  4. 3.6V

 

It is possible that all of them  exists or only some of them.

  1.  Could i use two ltc4413-2 components by shorting the outputs of them.
  2.  Are there  any special recommendations to this design? 

Thanks

Elyasaf