LT8610
Production
The LT8610 is a compact, high efficiency, high speed synchronous monolithic step-down switching regulator that consumes only 2.5μA of quiescent current...
LT8610 on Analog.com
LT8641
Recommended for New Designs
The LT8641 step-down regulator features Silent Switcher architecture designed to minimize EMI/EMC emissions while delivering high efficiency at frequencies...
Datasheet
LT8641 on Analog.com
LTC7151S
Production
The LTC7151S is a high efficiency monolithic synchronous buck regulator capable of delivering 15A to the load. It uses a phase lockable controlled on-time...
Datasheet
LTC7151S on Analog.com
Hello
I run the latest release of LTPowerCAD on my two PC, on windows 10 64b.
When I try to open a design for example LT8610 or LT8641, it crashes. If I try to open the file directly from the installation folder, I have an error window identical to the screenshots you can find on others topics related with this kind of issue.
I uninstalled SQL server and the simulator, reinstalled it, same problem. I run everything in adminstrator mode. Note that I don't have the problem with some parts, for example LTC7151S, it works well in this case I can open the default solution or a custom old one.
I have this problem on both computers. Looks like recent updates on windows introduced some incompatibilities with your software...because I don't remember having such issues some months ago.
Thanks
Aurelien
Hello. I recently downloaded LTPowerCAD II v2.7.3 and it is displaying the same crashing problem.
When I attempt to open ANY past LTPowerCAD files that I had designed a year ago or so, none of them will open, regardless of what IC it is simulating.
I even just created new files with just some random, fairly simple switching ICs (LT8604 and LT8619). When asked if I wanted to start with the default design file I said 'yes'. Without changing anything, I confirmed that the simulations were working correctly. And then promptly saved them without making any changes. When I attempted to open these default designs, they still crashed.
I did a full uninstall and re-install of the program, and it still displays the same problem.
Does anybody have any recommendations for this?
Hello. I recently downloaded LTPowerCAD II v2.7.3 and it is displaying the same crashing problem.
When I attempt to open ANY past LTPowerCAD files that I had designed a year ago or so, none of them will open, regardless of what IC it is simulating.
I even just created new files with just some random, fairly simple switching ICs (LT8604 and LT8619). When asked if I wanted to start with the default design file I said 'yes'. Without changing anything, I confirmed that the simulations were working correctly. And then promptly saved them without making any changes. When I attempted to open these default designs, they still crashed.
I did a full uninstall and re-install of the program, and it still displays the same problem.
Does anybody have any recommendations for this?
I've fixed the problem. I did a full uninstall, again. And downloaded the latest version again. This time when I opened it, it showed the version being v2.7.6 instead. Also, when I installed it this time, I ran the install setup file with administrator rights.
I don't know if was the newer version that fixed it or installing it as an administrator. But this seemed to fix the problem.