Post Go back to editing

LT3825 Flyback Transformer Inductance - Eval Schematic

Hi All,

I'm working on an LT3825 design for a 60W 12V output PoE PD. I'm using the 894C-C eval schematic as a reference. The schematic uses a Pulse PA1736NL transformer, which has a 20.5uH primary inductance. Using the LT3825 datasheet calculations this seems a very low value and would result in a very high ripple current when operating at the 200KHz. My calculation comes up with something around 170uH. 

I'm not that familiar with flyback converters, but I would think that the primary side of the transformer should work pretty much like a straight buck converter. Can anyone help me out here - the Eval board obviously works OK, so I must be missing something basic about how the transformer works?

Any help much appreciated.

Julian