Post Go back to editing

LT3825 Flyback Transformer Inductance - Eval Schematic

Hi All,

I'm working on an LT3825 design for a 60W 12V output PoE PD. I'm using the 894C-C eval schematic as a reference. The schematic uses a Pulse PA1736NL transformer, which has a 20.5uH primary inductance. Using the LT3825 datasheet calculations this seems a very low value and would result in a very high ripple current when operating at the 200KHz. My calculation comes up with something around 170uH. 

I'm not that familiar with flyback converters, but I would think that the primary side of the transformer should work pretty much like a straight buck converter. Can anyone help me out here - the Eval board obviously works OK, so I must be missing something basic about how the transformer works?

Any help much appreciated.

Julian

Parents
  • Hello Julian, There are multiple solutions for a Flyback. The best advise is on page 15 of the the LT3825 Data Sheet which suggests "A simple spreadsheet program is useful for looking at trade-offs." For a transformer, N * A * B = L* I. In this case, 170uH would require 5 to 6 times more turns (N) or core area (A). Everyone likes (their own) rules of thumb. For a Flyback, I check the ratio of the peak secondary current to the output current. In this case, with 20uH, this is about 15A / 5A ( = 3:1) which isn't too high. Good Luck.

Reply
  • Hello Julian, There are multiple solutions for a Flyback. The best advise is on page 15 of the the LT3825 Data Sheet which suggests "A simple spreadsheet program is useful for looking at trade-offs." For a transformer, N * A * B = L* I. In this case, 170uH would require 5 to 6 times more turns (N) or core area (A). Everyone likes (their own) rules of thumb. For a Flyback, I check the ratio of the peak secondary current to the output current. In this case, with 20uH, this is about 15A / 5A ( = 3:1) which isn't too high. Good Luck.

Children
  • Hi Kurk,

    Thanks for your reply. On your advice I have started to build a spreadsheet for all the calculations and it does shed light on things. I have also downloaded a complete LTSPICE simulation and played around with that looking at transformer currents etc. Really useful for understanding these things and remarkably accurate.

    For me it's a new area, I'm very happy with boost and buck converters, I just need to get more experience and as you say get some rules of thumb for the isolated converters.

    Thanks

    Julian

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.